Explore Types Of Ball Bearings And Their Applications
EnQuire Now
Types of Ball Bearings and Their Applications

Types of Ball Bearings and Their Applications

Posted date: 2024-06-05 12:04:46

Bearings — they are one of the essentials in the machinery component group. These materials are mandated to enable rotational and linear movement in machines that automatically reduce friction. Bearings are available in various shapes and sizes, which have specific functionalities. These bearings can be used in various industrial applications, including the automotive space, the construction industry and even aerospace.

All bearings have specific purposes, and in this blog, we will understand the varied types of bearings, their applications, and how they can make a difference in the working of your machinery. The definitive purpose of a bearing is to support the rotational shaft and help increase your machine's longevity. Remember, before purchasing or investing in quality ball bearings, understand the brand value and how long they have been catering to any particular industry requirements.

 

Angular Contact Ball Bearing

The angular contact ball bearings have both inner and outer ring raceways. These are designed to accommodate combined loads and, at the same time, act upon radial and axial loads. The load-carrying capacity of these bearings increases as the contact angle increases. According to a report, these bearings are defined as “Angular contact bearings are commonly used in gearboxes, pumps, electric motors, clutches, and other high-speed applications.”

 

SKF offers:
 

Single-row angular contact ball bearings

  • These bearings have high-loading capacity

  • These can be mounted very easily


 

Double-row angular contact ball bearings

  1. These bearings have less axial space

  2. They can be used for radial and axial loads in either direction. 

  3. They have stiff-bearing arrangements

  4. They are usually used when the single-row angular contact ball bearings aren’t enough

 

Four-point contact ball bearings

  1. It helps to cater to axial loads in two directions

  2. There is less axial space

  3. They take up less space compared to double-row bearings

  4. Accommodates axial loads in both directions

  5. They have a very high load-carrying capacity

  6. They can be separated

  7. It can be easily mounted or dismounted

  8. Improved oil flow

 

Deep Groove Ball Bearing

The most common and widely used bearing type, the deep groove ball bearing, is versatile. They ensure low friction, low noise and low vibration, such that they bring high speeds in machines’ rotation capacities. They are easy to mount on machines and require very little maintenance as compared to the other bearing types.

SKF is one of the trusted brands which offers a large variety of designs and variants in bearings. SKF goes beyond the catalog offerings and ensures that it caters to customizable bearings and provides applications that can meet specific needs.

 

Self-aligning Ball bearing

Need a solution to the moving shafts and misalignments? Self-aligning ball bearings can be apt for solving this problem. For years, SKF’s self-aligning ball-bearing has been constantly developed and also generates less frictional heat and can cater to higher speeds, depending on the size and the type as well. SKF also provides customized variants to accommodate every requirement, as per the industry demands. Therefore, depending on the requirements and the usage, SKF offers a wide assortment of sealed self-aligning ball bearings, which are also greased beforehand under very clean conditions.

SKF is one of the renowned brands in the ball bearings industry that has provided exceptional services to its customers for over 100 years. If you wish to order or explore bearings online, head to the SKF website for more information on the same. You’ll find elaborate product catalogues that will help you decide on your bearings requirements.

Over the years, SKF has also introduced and launched brands to enable a world of ‘reliable rotation’. They are constantly innovating and researching to match up to the growing demands of varied industries needing ball bearings, lubrication, and sleeves. Today, SKF has 103 manufacturing units worldwide, with a growing presence in over 130 countries.

Tags: balls Bearing , ball bearing types , ball bearing manufacturer , bearing pricing , Deep Groove Ball Bearing , Angular Contact Ball Bearings , SKF Ball Bearings , Roller Bearing , roller bearing types , Spherical roller bearings , Tapered Bearing , Cylindrical Roller Bearing , Types Bearings , Types of Bearings , SKF Bearings , Single Row Deep Groove Ball Bearing , Skf Deep Groove Ball Bearing , Deep Groove Ball Bearing are Used For , Deep Groove Ball Bearing Size Chart

Default Image

Author: Skf e-marketplace